Part Number: TMS320F28335
Hello,
I have to rework an old design.
I got a prototype from a colleague of mine.
I try to re-flash the DSC but I get the following message:
C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: C:\Users\USER\Local_repositories\project\Release\project.out: Load failed.
However, I can read and modify the contents of the RAM with the JTAG probe.
Is there a way to overcome this problem?
Thanks in advance
Steve