Part Number: TMS320F28062
Dear team:
My customer uses two F28062 chips for engineering development. Both chips use CPUtimer to define a task with a running cycle of 1ms. The entire program is executed sequentially and then waits for the main interrupt to execute again. Among them, the master also has a higher priority interrupt for high-frequency calculations, while the slave does not have this interrupt, only a 1ms interrupt.
SPI is used for communication between the two chips, and there will be about 30 16-bit data for interaction between the master and slave. That is, SPI dual-computer communication is realized in a program that runs periodically, receiving interrupts and sending without interrupts.
How to set up to ensure that 30 16-bit data SPI transceivers can be sent and received under the premise that the cycle stability does not affect other functions and real-time performance, and the transmission must also ensure the same periodicity?
Best regards