Part Number: TMS320F280049C
Hi There,
I'm observing a low drive strength on GPIO23 of my 280049C device in TQFP100 package. In particular, when sinking current, I'm seeing ~200uA over a 10k pull-down, which was directly measured, resulting in ~1V at the IO when being driven LOW.
I'm aware that this pin is used for a DC-DC converter, and have disable the "analog" function to allow it to operate as a normal GPIO. I have confirmed at a register level that the appropriate bits of the GPAAMSEL are set to '0', and have tried toggling the pin several times well after boot-up and configuration to see if that helped.

Here is my configuration of the pin:

Note that this pin is specified for 4mA source and sink capability, so I find this behaviour a bit perplexing:

This issue is absolutely critical and hitting an important programme, so would appreciate a fast response.
Thanks,
-Doug