Part Number: TMS320F28388D
Hello Community,
I'm able to import tcpEchoF2838X project and after making necessary changes able to build it in without errors.
I'm able to add driverlib_cm and add IPCISR as well.
But When I tried to run in debug mode I'm getting "Cortex_M4_0: AutoRun: Target not run as breakpoint could not be set: _JobHardwareBreakpoint::ARM_DEBUG_V7M_fpb_add_breakpoint: FPB : All resources are in use.[25062]" Error and execution halts.
This is my project folder :

This is my linker filer :
MEMORY
{
/* Flash sectors */
CMBANK0_RESETISR : origin = 0x00200000, length = 0x00000008 /* Boot to Flash Entry Point */
CMBANK0_SECTOR0 : origin = 0x00200008, length = 0x00003FF7
CMBANK0_SECTOR1 : origin = 0x00204000, length = 0x00004000
CMBANK0_SECTOR2 : origin = 0x00208000, length = 0x00004000
CMBANK0_SECTOR3 : origin = 0x0020C000, length = 0x00004000
CMBANK0_SECTOR4 : origin = 0x00210000, length = 0x00010000
CMBANK0_SECTOR5 : origin = 0x00220000, length = 0x00010000
CMBANK0_SECTOR6 : origin = 0x00230000, length = 0x00010000
CMBANK0_SECTOR7 : origin = 0x00240000, length = 0x00010000
CMBANK0_SECTOR8 : origin = 0x00250000, length = 0x00010000
CMBANK0_SECTOR9 : origin = 0x00260000, length = 0x00010000
CMBANK0_SECTOR10 : origin = 0x00270000, length = 0x00004000
CMBANK0_SECTOR11 : origin = 0x00274000, length = 0x00004000
CMBANK0_SECTOR12 : origin = 0x00278000, length = 0x00004000
CMBANK0_SECTOR13 : origin = 0x0027C000, length = 0x00004000
C1RAM : origin = 0x1FFFC000, length = 0x00001FFF
C0RAM : origin = 0x1FFFE000, length = 0x00001FFF
BOOT_RSVD : origin = 0x20000000, length = 0x00000800 /* Part of S0, BOOT rom will use this for stack */
S0RAM : origin = 0x20000800, length = 0x0000F7FF
E0RAM : origin = 0x20010000, length = 0x00003FFF
CPU1TOCMMSGRAM0 : origin = 0x20080000, length = 0x00000800
CPU1TOCMMSGRAM1 : origin = 0x20080800, length = 0x00000800
CMTOCPU1MSGRAM0 : origin = 0x20082000, length = 0x00000800
CMTOCPU1MSGRAM1 : origin = 0x20082800, length = 0x00000800
CPU2TOCMMSGRAM0 : origin = 0x20084000, length = 0x00000800
CPU2TOCMMSGRAM1 : origin = 0x20084800, length = 0x00000800
CMTOCPU2MSGRAM0 : origin = 0x20086000, length = 0x00000800
CMTOCPU2MSGRAM1 : origin = 0x20086800, length = 0x00000800
}
SECTIONS
{
.resetisr : > CMBANK0_RESETISR | CMBANK0_SECTOR0
.vftable : > CMBANK0_SECTOR0 /* Application placed vector table in Flash*/
.vtable : > S0RAM /* Application placed vector table in RAM*/
.text : >> CMBANK0_SECTOR4 | CMBANK0_SECTOR5
.cinit : > CMBANK0_SECTOR0
.pinit : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.switch : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.sysmem : > S0RAM
.stack : > C1RAM
.ebss : > C1RAM
.econst : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.esysmem : > C1RAM
.data : > S0RAM
.bss : > CMBANK0_SECTOR6
.const : {} LOAD = CMBANK0_SECTOR9 | CMBANK0_SECTOR10 ,
RUN = S0RAM,
LOAD_START(constLoadStart),
LOAD_SIZE(constLoadSize),
LOAD_END(constLoadEnd),
RUN_START(constRunStart),
RUN_SIZE(constRunSize),
RUN_END(constRunEnd),
ALIGN(8)
MSGRAM_CM_TO_CPU1 : > CMTOCPU1MSGRAM0, type=NOINIT
MSGRAM_CM_TO_CPU2 : > CMTOCPU2MSGRAM0, type=NOINIT
MSGRAM_CPU1_TO_CM : > CPU1TOCMMSGRAM0, type=NOINIT
MSGRAM_CPU2_TO_CM : > CPU2TOCMMSGRAM0, type=NOINIT
.TI.ramfunc : {} LOAD = CMBANK0_SECTOR0 | CMBANK0_SECTOR1 | CMBANK0_SECTOR4,
RUN = S0RAM,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
My debug properties:

Error:


Include options :

I have also gone through certain forum threads but they didn't help.
My ultimate goal is to - Bring Up TCP/IP and communicate between a Host and Client and further send and receive certain set of commands
Note: I'm able to communicate using with a Host PC using UDP but I dont want to use UDP.
Please let me know how would I achieve this ?
Regards,
Pranay