Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
Hi team,
Here's an issue from the customer may need your help:
A single phase inverting UPS that customers are doing now.
The peak of the output at no load corresponds to the value of the H-bridge Vbus (which was developed with 48V) multiplied by the modulation ratio, but with a pure resistance of 25R, it was found that the peak of the inverting AC wave was about 5 V lower than the product of the Vbus and modulation ratio.
a. What does this drop relate to?
b. Is power control calculated by apparent power or average power?
c. Where can they find the calculation of power in my code?
d. Is the CBC function enabled when there is also overcurrent? How is overcurrent controlled?
e. How is the power calculated when the load is an inductive load? Does the code for this project have a calculation of the phase?
Could you help check this case? Thanks.
Best Regards,
Cherry