Part Number: TMS320F280025C
Hi expert,
I want to configure CMPSS module with two thresholds per comparator. I see on the datasheet, there is an option to use hysteresis on the input. I configure CMPSS by DAC value on the negative input comparator, so I want set a trigger condition and untrigger condition (if INPUT_PIN1 > THRESHOLD1 then ePWM is OFF and ePWM is ON when INPUT_PIN1 < THRESHOLD2). The difference between THRESHOLD1 and THRESHOLD2 on voltage is 100mV knowing that the full scale input is 3.3V.
So it's an hysteresis on CMPSS input, Is it possible to configure that ?
Thanks
Damien