Part Number: TMDSCNCD28388D
Using CCS11.0.0
I have some global variables that are used by external tools to control the software and they are being optimized out of the map file.
I am using a simple OS that calls the tasks from a function pointer. Somehow the code thinks that the task with the call to a function that manipulates the variable is not called so optimizes out the variable name. If however I add a call to a function that uses the variable it gets included in the map file.
My question is there a compiler/linker option to keep the global symbols? As of yet, I have been able to locate the option yet.
Here is the warning:
2838x_flash_lnk_c28x.cmd", line 168: warning #10068-D: no matching section
Here is the section declaration
IRAM : { *(.code_checkMemClassRam) *(.IRAM_Var) *(.IRAM_DATA) *(.IRAM_measure_variables) }> RAMGS1 , ALIGN(4)
I am using the same pragma's to declalre the sections in the code and only the code_checkMemClassRam is optimized out.