Part Number: TMS320F280025
Please take a look at the 280025 configuration. Please pay attention to the following points: (1) whether the matching of all power capacitors is reasonable. (2) Configure pin 4 as the input positive of cmpss and as overcurrent protection. Use internal DAC to set the overcurrent protection threshold. Is this reasonable. (3) Whether the 23 and 24 pins are configured as can communication pins is reasonable. (4) Whether the use of crystal oscillator and the setting of writing port are reasonable. (5) Whether the input and output of pin 1 and 2 configured as Lin communication is reasonable. thank you!