Part Number: TMS320F280049C-Q1
Hi everybdoy ,
please I need confirmation on lock registers and if I can reset and rewrite
in particular
- I m ok with COMPLOCK register ( 16.7.2.21 offset = 1Ah ) . I can write once and I can reset ( so I can write again ) after a SYSRSn system reset -->OK
- now consider TRIPLOCK register ( 9.3.4.26 ) , here it looks access is still RWSonce but not clear stated you can reset ONLY via a SYSRs : is it the same as COMPLOCK?
- same for EPWMLOCK : is it the same as COMPLOCK
thank you for the confirmation
BR
Carlo