Hi all!
As I mentioned can we disable high resolution feature of the EPWM modules when not needed? It seems we don't need high pwm during prototyping but need quick solution. Thats why don't wanna deal with high res features.
Also what is the maximum resolution of EPWM module for both cases? For example for 80kHz PWM what is the max available resolution with HRPWM or non HRPWM?
Thanks in advance.
cheers,