Part Number: TMS320F280049C
Hello
We want to speed up the start-up of a motor by giving forced angle a known start value. The rotor position is determined by HALL sensors but the update rate is too low to run the motor,
but the starting position is stable.
There is a function to set the angle of "Forced Angle" but it seems that then also the delta value is adjusted resulting in a very high frequency, instead of the 1 Hz.
Is it possible to speed up the startup in this way, or are there other options?