Part Number: TMS320F28388D
Hello,
I am using TMS320F28388D control card.
I wrote a simple code to enable SPIA with 8 bit and 1MHz frequency .
The code is building but while flashing the code to controller its getting terminated at the below function call in sysctl.h
SysCtl_delay(23U);
The above function is called while configuring the system Clock.
Is there any configuration that need to be done in the workspace of the project.
Any input on this will be helpful.
Also attaching the error screen.
Thanks
Navya Anna Prince