Part Number: TMS320F28055
Other Parts Discussed in Thread: C2000WARE,
I am in deep stuck with a programming issue. Can anyone help me?
Chip: TMS320F28055PNT
Programmer/Debugger: XDS200/XDS110 using 10 pin connector.
Programming connection of the microcontroller as below:

10 pin programming connectors for programmer as below:

I am getting the below error.

I observe that there is no output from TDO Pin of the controller.
I change Trst pin pull down to 10K instead 2.2K
still getting error.
Is there anything more, I am missing?