Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: BOOSTXL-DRV8301, DESIGNDRIVE, C2000WARE, CONTROLSUITE, SFRA, DRV8301, BOOSTXL-3PHGANINV
Hi Team, assisting a customer seek some clarifications.
Trying to make a BLDC with hall sensors work with a TI lauchpad (LAUNCHXL-F28379D) and a boosterpack (BOOSTXL-DRV8301). Considering the presence of both a C2000 Delfino mcu and digital Hall sensors on the motor, I excluded the use of INSTAspin solutions all together, as they work on C2000 piccolo mcu ideally for sensorless motors.
What is left is the Designdrive software package which, if I understood correctly, is now supported via the C2000ware package + Motorcontrol SDK. Before, on the other hand, it was included in the controlsuite package which is now not updated anymore.
Questions are:
• Can I still use controlsuite with this board for this work or do I have to move to C2000ware+SDKs solutions?
• From the pdf “controlSUITE to C2000Ware Transition Guide” I learnt that everything that was included in controlsuite is now available with C2000ware+the appropriate SDK. However I can’t find the same examples I could locate in the controlsuite package at all (e.g. C:\ti\controlSUITE\libs\app_libs\motor_control\libs\FCL_SFRA\v01_00_00_00\Examples\FCL_SFRA_379DXL_v1\~Docs). Where can I find them on the newer C2000ware environment?
• Are there examples of motor configuration and connections, hall readings, encoder configurations, controllers available? I mean, for instaspin solution there is a series of labs which guide you through the implementation of softwares, is there something like that for designdrive too?
Thank you in advance.
-Mark