Part Number: TMS320F280041C
Other Parts Discussed in Thread: DRV832X, DRV8323
Good Afternoon,
We are implementing a new FOC BLDC design with the F280041C and DRV832x driver. The question we have is how to determine choosing either the MCU's PGA or the driver's CSA to amplify our current sense voltage and which has better performance/efficiency? Is there ever a case when it would it would be beneficial to use both? Example: Very low current lets say 200mA. Instead of increasing shunt resistor size and decreasing efficiency, would it better to use CSA's 40V/V and PGA's 25V amplifiers? (0.2A x 0.002 shunt x 40 CSA x 25 PGA) = 0.4V
TIA
Best,
Jonathan