Part Number: TMS320F280025C
Other Parts Discussed in Thread: C2000WARE, C2000WARE-MOTORCONTROL-SDK
Dear Team,
I have designed one customized hardware for BLDC motor to control speed using Hall sensor. [used sensor trapezoidal method ]
I have applied PWM based on Throttle input [ Throttle is connected to ADC pin ].
For current sensing I have used current sensing IC and I able to measure current consume by the device also I have used capture module to measure speed of the BLDC.
Motor parameters:
RPM max : 4000
Motor operating Voltage: 24VDC
My problem is I have to apply external force to motor at initial condition [ without external force motor is not START rotating ]
I want to control motor speed at very low RPM with desired torque
Please guide me how to start motor at initial stage [ without external force ] and also I want to know how to control motor speed at very low RPM with desired torque?
I have used C2000ware example for software development.
Best and regards,
Dipak