Part Number: TMS320F280049
Other Parts Discussed in Thread: CC2652RSIP, CC2650MODA, CC2652R7
I am currently using an '0049 processor in a prototype product with motor control. I have it talking to a Nordic NRF processor which is handling supervisory functions and has built-in bluetooth. It seems crazy to have two processors for this low-cost application.
1. Does TI have a processor with built in Bluetooth that can do motor control. (having PWMs, ADCs, Preferably eQEPs, etc)?
2. What external Bluetooth options are available to easily interface with a C2000 (or another) TI microcontroller?
3. The NRF has FCC approval. If you suggest some options, Which solutions would require FCC approval?
4. if I go with a C2000 processor and external bluetooth, what part(s) would you suggest?
Regards
Neil