This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: PWM for a Single-Phase H Bridge Inverter

Part Number: TMS320F28379D


Hello,

I want to use TMS320F28379D LaunchPad to generate high frequency PWM for my single-phase H bridge inverter. 

Do you think it is possible to generate a PWM with frequency of 1.5MHz for th carrier signal and 150kHz sine wave for the duty cycle with good resolution?

I've tried to do so using DSP Sine Wave block in Simulink and the maximum resolution I've got for the duty cycle was 20 points per cycle for 20kHz (maximum sampling time was 25us).

Thanks in advance for your help 

MJ