Part Number: TMS320F280049
Hello,
I want to connect a dual synchronous sampling ADC (AD4680) to the TMS320F280049 (Master) via SPI. The ADC has two data output lines. Can I configure the SPI module of the microcontroller in a way to read both data lines simultaneously? Or do I need to connect each data channel to a different SPI module in the microcontroller and synchronize them somehow?
Thank you
Sebastian