Part Number: TMS320F28374D
Other Parts Discussed in Thread: TMS320F28388D, SYSCONFIG, C2000WARE, TMS320F28335
Hi Experts,
I am posting this inquiry on the behalf of our customer. Kindly see the message below:
"I am trying to configure pins of some of the MCU chips (TMS320F2837x or TMS320F2838x) picked up as candidates for the core of our new ECS modules, required by pending power converter control projects and some similar applications.
At the final stage of the configuration process (regardless of S or D versions of previously mentioned MCU chips), i.e. after I have assigned most of the MCU subsystems to the available pins (of the 337pin package), when I try to add one more subsystem (either McBSP or I2C port) design software crashes reporting "Oh Snap! The last change caused an exception" message (see attached image). I double-checked few times, that all required pins at which those interfaces (e.g. either of ports I2C-A, I2CB, McBSP-A, McBSP-B etc.) are normally available, are still unassigned!
Used SysCfg files, demonstrating this issue, are also attached to this message.
The same EXCEPTIONall crash issue pops-out when using that "TI System Configuration Tool" software for the pin assignment of the F2838x MCU chips (also 337-pin package version).
Besides, it would be nice to know if users should be afraid of the fact that there are separate Tool configuration options for single- and dual-core versions of F2837x microcontrollers (FS2837xS and F2837xD), while there is only one Tool configuration option for F2838x series of Delfino microcontrollers.
P.S: There are still several other issues related to the concurrent usage of particular subsystems available within TMS320F28388D MCUs (but first things first...)
Additionally, I wanted to point out that I appreciate "resource conflict" warnings, which occasionally occur when I try to combine other unsupported subsystem combinations (due to incompatible pin assignments)."
Below is the screenshot of the error and the sysconfig files mentioned. Kindly have a look.

Would you kindly help with this inquiry?
Thank you.
Regards,
Marvin