Other Parts Discussed in Thread: TMS320F280200
Hi There
I just came across the TMS320F280200. I have downloaded the ePWM ref guide in relation to this, but I note that it is very detailed and will take quite a bit of reading...
I would like to check suitability of this device before spending the afternoon reading the pdf, so if anyone has familiarity with this device could you tell me if it is able to generate a PWM signal with frequency that varies from 0.1MHz to 50MHz and with a duty cycle that varies continuously (or at least with a pretty high resolution) from 0% to 100% at the lower frequencies and a reduced range around 50% at the high end...?
Very much appreciated to save my time learning if is not suitable, thanks you.