Part Number: TMS320F280023C
Other Parts Discussed in Thread: C2000WARE
Hi,
I have set up SOC2 on my microcontroller to trigger on the ePWM1 SOCA output signal.
There is a varying voltage on my input pin (A2), but despite the ISR being entered frequently (checked with a counter variable) the value of the ADC result register doesn't change. It just stays fixed at 2045-2046.
Here is my initialisation code and ISR code. Please help me figure out what I'm missing.
void init_adc(void)
{
EALLOW;
CpuSysRegs.PCLKCR13.bit.ADC_A=1;
EDIS;
ADC_setVREF(ADCA_BASE, ADC_REFERENCE_INTERNAL, ADC_REFERENCE_3_3V);
EALLOW;
AdcaRegs.ADCCTL1.bit.ADCPWDNZ=1; // Power on the ADC
AdcaRegs.ADCCTL2.bit.PRESCALE = 2; // ADCCLK=50MHz for SYSCLK=100MHz
//SOC2: triggered by EPWM1-SOCA, 270ns acquisition window, sampling on channel 2
AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = 0x5;
AdcaRegs.ADCSOC2CTL.bit.ACQPS = 26;
AdcaRegs.ADCSOC2CTL.bit.CHSEL = 2;
AdcaRegs.ADCCTL1.bit.INTPULSEPOS=1; // Interrupt pulse generation occurs at the end of conversion, 1 cycle before result latching on to the result reg
AdcaRegs.ADCINTSEL1N2.bit.INT2SEL=2; // Set EOC2 as interrupt trigger for ADCINT2
AdcaRegs.ADCINTSEL1N2.bit.INT2CONT=0;
AdcaRegs.ADCINTSEL1N2.bit.INT2E=1;
EDIS;
DEVICE_DELAY_US(5000);
}
__interrupt void ADC2_ISR(void)
{
adcval_raw = AdcaResultRegs.ADCRESULT2;
adcval = 3.3*(((float)adcval_raw)/4096);
soaCurrent = ((1.65-adcval)/(20*0.004));
EPwm1Regs.ETCLR.bit.SOCA=1;
AdcaRegs.ADCINTFLGCLR.bit.ADCINT2=1;
PieCtrlRegs.PIEACK.bit.ACK10=1;
}
Thanks in advance.
Regards,
Vishnu