This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: Failure in the TRM

Part Number: TMS320F280049

Hello experts,

there is an failure in the TRM (SPRUI33D):

"GPIO19" is not available, but it is listed in the following tables and figures:

Figure 8-6. GPAQSEL2 Register
Table 8-13. GPAQSEL2 Register Field Descriptions
Figure 8-8. GPAMUX2 Register
Table 8-15. GPAMUX2 Register Field Descriptions
Figure 8-9. GPADIR Register
Table 8-16. GPADIR Register Field Descriptions
Figure 8-10. GPAPUD Register
Table 8-17. GPAPUD Register Field Descriptions
Figure 8-11. GPAINV Register
Table 8-18. GPAINV Register Field Descriptions
Figure 8-12. GPAODR Register
Table 8-19. GPAODR Register Field Descriptions
Figure 8-15. GPAGMUX2 Register
Table 8-22. GPAGMUX2 Register Field Descriptions
Figure 8-18. GPACSEL3 Register
Table 8-25. GPACSEL3 Register Field Descriptions
Figure 8-20. GPALOCK Register
Table 8-27. GPALOCK Register Field Descriptions
Figure 8-21. GPACR Register
Table 8-28. GPACR Register Field Descriptions
Figure 8-47. GPADAT Register
Table 8-56. GPADAT Register Field Descriptions
Figure 8-48. GPASET Register
Table 8-57. GPASET Register Field Descriptions
Figure 8-49. GPACLEAR Register
Table 8-58. GPACLEAR Register Field Descriptions
Figure 8-50. GPATOGGLE Register
Table 8-59. GPATOGGLE Register Field Descriptions

The GPIOs 36 and 38 are not available too and they are marked in the corresponding registers as "reserved".
This should also be done with the GPIO19.

Regards,

Jan