Part Number: TMS320F280025-Q1
Other Parts Discussed in Thread: C2000WARE
Hi Experts,
Let me clarify about the Flash API usage.
TMS320F28002x Flash API Version 1.57.00.00 (spnu631) says "TMS320F28002x Flash API is embedded into the Boot ROM of this device. This differs from other C28x devices where the API is wholly software."
a) The Flash APIs in ROM do not need to be copied to the RAM and Flash APIs in ROM are called directly by the user program in RAM. Am I correct?
b) Does all user program including the using ISRs except the Flash APIs have to be copied to RAM and executed for Flash erase/program?
c) With the other device F28034, the Flash API had to be copied to the RAM. It seemed that the Flash APIs are located in the ROM with F28034 too. Please clarify.
Thank you for your check.
Best regards,
Hitoshi Sugawara