Other Parts Discussed in Thread: TMS320F280025
Hello,
Is there any low cost C2000 device which has 9 independent timers?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS320F280025
Hello,
Is there any low cost C2000 device which has 9 independent timers?
Regards,
While all the C2000 have 3 CPU timers, the PWM modules can act as independent timers as well. So a device like the TMS320F280025 which had 7 ePWM modules, would have 10 independent timers on-chip. A PWM module can be configured, but the PWM signal doesn't need to be brought to a pin, so in this way it can act as a timer.
If the PWM modules are needed for PWM function, then we would need to look at a device with more PWMs, that could be used as timers in addition to the 3 CPU timers.
Best,
Matthew