Part Number: TMS320F28388D
Other Parts Discussed in Thread: PSPICE-FOR-TI, TINA-TI
Hello,
I am trying to design ADC circuit for the specified part number. I need a sample rate of 100 KSPS to measure the input voltage range of 0 to 30 V. The input voltage is fed to the ADC after a resistor divider. As I understand I will have to implement buffer and RC filter between the divider and the ADC to isolate the high impedance of the divider. I would like to know for the given sample rate, how much resistance/ impedance can I use so I can avoid using the buffer op amp. Is it possible or buffer has to be included?