Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Hi,
I imported one of the examples into my workspace ex2 - Shared LED Blink
It adds 2 projects namely - freertos_ex2_shared_led_blink_cm AND freertos_ex2_shared_led_blink_cpu1
The CM project as per my understanding is the COMMUNICATION MANAGER.
Questions:
`. Is there a particular way in which these projects need to be loaded on the board? (For example when using dual core one project is loaded on CPU1 and other on CPU2, how does the loading with FreeRTOS work?)
2. Is there a guide to getting started with these FreeRTOS examples?
3. When I try to build the CM project FreeRTOS.h file is missing, from where can I download this file?

Thanks & Regards,
Rashmitha