This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Sent & receive Data with J1939 Stack

Part Number: TMS320F28379D


We are using Sys Config Tool for defining object ID for CAN message. I am integrate J1939 stack first time with CTS/RTS. I have one Message Object define as below which send RTS and Data. 

CAN_setupMessageObject(CANB_BASE, 5U, 470177524, CAN_MSG_FRAME_EXT,CAN_MSG_OBJ_TYPE_TX, 0, 0,8);

In order to read CTS I need to read CAN buffer. is it possible to receive all CAN data and pass to J1939 Stack or is there any way to implement CTS data reading. 

  •  Aashwita,          

                    We are happy to help in questions pertaining to modules on our device. For J1939 questions, you may want to reach out to J1939 forums. We regret we cannot help you with that.

    is it possible to receive all CAN data

    If you are asking if it is possible to receive all message IDs in a message object, the answer is 'yes'. Please refer to the mask example in www.ti.com/lit/sprace5