Part Number: TMS320F28054M
Hi team,
Here's an issue from the customer may need your help:
1) with 28054 for position control, the customer only has 28069 demo board, so uses 28069 for parametric identification. Then use the drv8301kit_revD> f2805xM> lab13b routine and change it to adapt to the self-made board(after the changes are done, parametric identification is not working properly, and the inertia identification program is working properly. The detected resistance value is abnormal if enable resistor to recalibrate while the position control is being performed. ), using a magnetic encoder, the motor operates normally without load, with a slight jitter with a large load (the motor performance is sufficient at a large load which is tested with other master's board).
There is no significant difference in adjusting the bandwidth by the upper computer looking at the given and following basic coincident of the current loop over the transmit and receive data frequency of 20 hz.
2) under inductive position control, dose EST_run(EST_Handle handle,const MATH_vec2 *pIab_pu,const MATH_vec2 *pVab_pu,const _iq dcBus_pu,const _iq Does the speed_ref_pu) need to be executed?
3) The observed value of the magnetic chain and the value of the magnetic chain identified with the 28069demo board also differ significantly during motor operation.
Could you help check this case? Thanks.
Best Regards,
Cherry