Other Parts Discussed in Thread: LAUNCHXL-F280025C, DRV8353RS-EVM, DRV8353, DRV8323, MOTORWARE
Hi,
I'm testing the universal motor lab using below HW.
Target Board : LAUNCHXL-F280025C
Motor Booster Pack : DRV8353RS-EVM
Motor : Anaheim_BLY172S_24V.
DC Bus : 24V
I checked adcData.VdcBus_V, Offset_I_ad, Offset_v_sf and PWM frequency.


These values are similar to Figure 2-25.
So I run the LEVEL2, but motor doesn't spin.
In the Motor Control SDK Universal Project and Lab user guide, motorVars_M1.speedRef_Hz and motorVars_M1.speed_Hz show different speed.
When the motor spins normally, the two values should be similar.
But both my tests and documentation have different values.

The expression below was captured when I tested LEVEL 2.
The graph shows current of motorVars_M1.adcData.I_A.value[0]