Part Number: TMS320F28075
Other Parts Discussed in Thread: TMS320F280023
Hi Experts,
Good day. We have this case from client about XDS110 which unable to program the target:
"I am trying to program a board that uses the F28075 chip. The XDS programmer returns various errors. And just does not program the boards.
I'm wondering whether that chip is supported by the XDS110.
IcePick_C_0: Error connecting to the target: (Error -267 @ 0x0) The controller could not detect valid target supply. Check target JTAG connection and/or connection setting specifying voltage level. (Emulation package 7.0.188.0)
Client update:
The person I talked with asked for an error message and that was the only one I had access to at the time. The fact is, the XDS 110 is NOT communicating with the board. I manage to program the board just fine with an XDS100. So clearly the issue is with the XDS110. I will try to communicate using the XDS110 and upload the appropriate errors.
These are the behaviors of the same board with different configurations. The XDS100 connected to the board with the default configurations. The XDS110 did not. You can see the connection properties on the right side of the images."
For your confirmation and assistance.
Thank you.
Regards,
Archie A.