This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Memory Map File Error

Part Number: LAUNCHXL-F28379D


Dear Sir,

I am working on Launch-XL-28379D. I have assigned .ebss section in Memory map file as below

.ebss            : >> RAMGS0|RAMGS1|RAMGS2|RAMGS3,    PAGE = 1

And my memory Allocation at building project is as below

From the above image , it shows that GS1, GS2, GS3 Sections are unused or Free or Available. Despite the error shown as i

Description Resource Path Location Type
<a href="file:/c:/ti/ccsv8/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x2555 page 1. Available memory ranges: 2837xD_RAM_lnk_cpu1.cmd /VCU_28379D_CPU01 line 79 C/C++ Problem

Please resolve this Issue

Thanking you

  • Hi,

    Pls share the linker command file. 

    Also , can you try specifying the memory allocation for .ebss section as below (without the PAGE specifier)

    .ebss            : >> RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3

    Best Regards

    Siddharth

  • MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN            : origin = 0x000000, length = 0x000002
       RAMM0            : origin = 0x000122, length = 0x0002DE
       RAMD0            : origin = 0x00B000, length = 0x002000
       RAMLS0           : origin = 0x008000, length = 0x000800
       RAMLS1           : origin = 0x008800, length = 0x000800
       RAMLS2           : origin = 0x009000, length = 0x000800
       RAMLS3           : origin = 0x009800, length = 0x000800
       RAMLS4           : origin = 0x00A000, length = 0x000800
       RESET            : origin = 0x3FFFC0, length = 0x000002
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x000121     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
       RAMD1           : origin = 0x00B800, length = 0x000800
    
       RAMLS5      : origin = 0x00A800, length = 0x000800
    
       RAMGS0      : origin = 0x00C000, length = 0x001000
       RAMGS1      : origin = 0x00D000, length = 0x001000
       RAMGS2      : origin = 0x00E000, length = 0x001000
       RAMGS3      : origin = 0x00F000, length = 0x001000
       RAMGS4      : origin = 0x010000, length = 0x001000
       RAMGS5      : origin = 0x011000, length = 0x001000
       RAMGS6      : origin = 0x012000, length = 0x001000
       RAMGS7      : origin = 0x013000, length = 0x001000
       RAMGS8      : origin = 0x014000, length = 0x001000
       RAMGS9      : origin = 0x015000, length = 0x001000
       RAMGS10     : origin = 0x016000, length = 0x001000
    
    //   RAMGS11     : origin = 0x017000, length = 0x000FF8   /* Uncomment for F28374D, F28376D devices */
    
    //   RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       RAMGS11     : origin = 0x017000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS14     : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS15     : origin = 0x01B000, length = 0x000FF8     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       
    //   RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
                                                                /* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */
    
       CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
       CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
    
       CANA_MSG_RAM     : origin = 0x049000, length = 0x000800
       CANB_MSG_RAM     : origin = 0x04B000, length = 0x000800
    }
    
    
    SECTIONS
    {
       codestart        : > BEGIN,     PAGE = 0
       .text            : >> RAMGS6 |  RAMGS7 | RAMGS8 | RAMGS9 | RAMGS10 | RAMGS11 | RAMGS12 | RAMGS13 |RAMGS14 |RAMGS15,   PAGE = 1
          //.text            : >> RAMD0 |  RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,   PAGE = 0
    
       .cinit           : > RAMGS5 ,     PAGE = 1
       .switch          : > RAMM0,     PAGE = 0
       .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
       .stack           : > RAMM1,     PAGE = 1
    
    #if defined(__TI_EABI__)
       .bss             : > RAMLS5,    PAGE = 1
       .bss:output      : > RAMLS3,    PAGE = 0
       .init_array      : > RAMM0,     PAGE = 0
       .const           : > RAMLS5,    PAGE = 1
       .data            : > RAMLS5,    PAGE = 1
       .sysmem          : > RAMLS5,    PAGE = 1
    #else
       .pinit           : > RAMM0,     PAGE = 0
       .ebss            : >> RAMGS0|RAMGS1|RAMGS2|RAMGS3,    PAGE = 1
       .econst          : > RAMLS5,    PAGE = 1
       .esysmem         : > RAMLS5,    PAGE = 1
    #endif
    
       Filter_RegsFile  : > RAMGS0,    PAGE = 1
    
    
       ramgs0           : > RAMGS0,    PAGE = 1
       ramgs1           : > RAMGS1,    PAGE = 1
    
    #ifdef __TI_COMPILER_VERSION__
       #if __TI_COMPILER_VERSION__ >= 15009000
        .TI.ramfunc : {} > RAMM0,      PAGE = 0
       #else
        ramfuncs    : > RAMM0      PAGE = 0   
       #endif
    #endif
    
       /* The following section definitions are required when using the IPC API Drivers */
        GROUP : > CPU1TOCPU2RAM, PAGE = 1
        {
            PUTBUFFER
            PUTWRITEIDX
            GETREADIDX
        }
    
        GROUP : > CPU2TOCPU1RAM, PAGE = 1
        {
            GETBUFFER :    TYPE = DSECT
            GETWRITEIDX :  TYPE = DSECT
            PUTREADIDX :   TYPE = DSECT
        }
    
        /* The following section definition are for SDFM examples */
       Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
       Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
       Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
       Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
       Difference_RegsFile : >RAMGS5,   PAGE = 1, fill=0x3333
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

  • Satish,

    Did you try changing the .ebss section to 

    .ebss            : >> RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3

    Best Regards

    Siddharth

  • Did you try changing the .ebss section to 

    .ebss            : >> RAMGS0 | RAMGS1 | RAMGS2 | RAMGS3

    Yes , Still the same issue persists. 

    stack size taken  = 0x200

    Heap Size taken = 0x100 

    and used different iterations of Optimisation levels

    please resolve this issue

  • Another option you can try is to combine the memory regions in the linker command file

       RAMGS0_3      : origin = 0x00C000, length = 0x004000 

    and then use it in the SECTIONS like this

    ebss            : > RAMGS0_3

    Best Regards

    Siddharth

  • Dear Sir, 

    I tried the same as above, still the same issue persists. 

    Please resolve this issue

  • Hi, 

    Can you share the compilaton log and project?

    Best Regards

    Siddharth

  • Sir,

    Please find the attached compilation log File .

    Project Log.txt

  • Hi, 

    If you read the log, you can find that the "..ebss" section size is 0x233e.  It needs a memory region which can accomodate this size. 

    Can you share your updated linker command file with RAMGS0_3      : origin = 0x00C000, length = 0x004000 ?

    Is there any other section that is allocated to RAMGS0_3?

    Best Regards

    Siddharth