This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Adapting universal motor control lab for RSH package

Part Number: TMS320F280049C


Hello,

In the lab manual for the universal motor control lab that comes with the motor control SDK (V3.03), chapter 3 shows how the lab can be adapted for other microcontrollers and gate drivers on custom boards. This sound quite promising, so I am giving it a look.

The board I am using has the F280049C microcontroller, but with the 56 pin RSH package instead of the usual 100 pin PZ package. I have changed the --package and --part flags for 56RSH in the build options but I cannot find where I can adapt the pin mux as necessary for this board. How does the pin mux work here and how can I adapt it to my board?

Cheers,

John