Part Number: TMS320F280039C
Hi Champ,
I am studying on PMBus, especially focus on PMBus over I2C master / slave.
I read the USER’S GUIDE of PMBus Communications Stack. Page57. shows the Master and slave configuration.
However, from my side the example projects (28003x_pmbus_over_i2c_master/slave), both of the examples couldn't compile successfully.
The example of PMBus_over_I2C_Master compiler error shows in below: (#10234-D: unresolved symbols remain)
The F28003x_PMBus_Communication_Stack.lib is added in the project. Not sure is it because the unresolved symbol's body isn't in the library ?
I am using CCS11.1.0 and the compiler version is v21.6.0.LTS.
Is the error because of the missing steps from me, result in the compiler error ? Or CCS/compiler version problem ?
Thanks for any help.
Johnny