Part Number: TMS320F280025C
I have been working with "TMS320F280025CPNSR" for motor control application. I want to know if the controller needs to start from the default boot mode (i.e. FLASH after reset), do I need to pull GPIO32 and GPIO24 to high. Will it be ok, if those pins are used as I/O GPIO pins but not pulled-high but still boot mode is default to FLASH mode.