Other Parts Discussed in Thread: TMDSCNCD28388D, DP83822I
Hi team,
Here're some issues from the customer may need your help:

1) As above description of PHY Reset Signal, here's 2 ways, one is the ESC and PHY synchronous reset, in which case the reset signal needs to be pulled down. Another mode is to release ESC and then PHY. In this way, the reset signal is the control of the IO and is controlled by the MCU. Is this correct?
2) When will the two reset modes be used? What are their prerequisites?
3) The following figure is the design in TMDSCNCD28388D, will GPIO155 require pulldown?

Could you help check this case? Thanks.
Best Regards,
Cherry