Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: C2000WARE, DP83822I
Dear team:
TMDSCNCD28388D: C:/ti/c2000/C2000Ware_4_00_00_00/boards/controlCARDs/TMDSCNCD28388D/Rev.B/MCU063B(002)_Sch.PDF
On page 8 of the above schematic diagram, 2.2k pull-up resistors (R127 & R152) are added to the MDIO pins of the two DP83822IRs and then connected to the GPIO153 of the F28388D:

However, Figure 31-5 on page 3301 of the chip TRM states: that MDIO must have a pull-up resistor (4.7 kOhm recommended) externally.

In this case, is the resistance value too small after the two 2.2k resistors on the schematic diagram of TMDSCNCD28388D are connected in parallel?
Best regards