Part Number: TMDSSOLARUINVKIT
Hi
I am working on the kit TMDSSOLARUINVKIT. I currently don't have access to a solar emulator. The recommended power rating of solar panel(140W) are too large to work on a home setup.
I want to operate the kit at minimum power level.
I have found a few solar panels:
In summary,
1) Can I operate the kit using the solar panel above?
2) Can I operate the kit at input voltage of 12V, power level of 50W.
3) Could you please recommend any other solar panel/emulator which I can use to operate the kit at a lower power level at home?
Thanks,
Mukul