Part Number: TMS320F280025
Hi,
We are currently looking at using the TMS320F280025 and it looks like it will fit our need , one thing i need to get clarity on is that according to the datasheet page 10 the following comment is made
"(2) C devices include additional Motor Control libraries in ROM. Contact TI for more information"
Question that i have is the following ,
1. is this programmed in the flash , and should it be included in code to be used or do you access the functions via some other means
2. if this is not part of the flash is it sitting in some other area , ie secure rom , and can it be over written by accident when flashing?
regards
C