Hi all,
I am working on a project which involve an F28379D, I designed my own control card and everything is ok.
I would like to know how can I program my µC in STANDALONE (via flash) but keep using debugger (without the need of turnin off / on the power supply).
At this moment I have the choice, if I program it in STANDALONE mode I can't use the debugger because I need to switch ON/OFF the µC, if I program it without the STANDALONE mode, I can use the debugger but if I turn OFF the supply my program will not run...
(I am using both CPUs I have a project for each one)
Thank you in advance !