Part Number: TMS320F280049
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE-MOTORCONTROL-SDK, C2000WARE, MOTORWARE
Hello C2000 gurus,
Do you have an EABI version of the eSMO library in ControlSuite? I am porting some old IQ math based code to F28004x. I want to continue using IQ math on F28004x for now. I would like to use the eSMO library that is in controlSuite with the F28004x project. This lib currently works with the old working code on an older Piccolo device.
The F28004x project uses a combination of driverlib and bit field headers and libraries. The project compiles, but the linker is giving me the following warnings and related eSMO undefined symbol errors (symbols that are defined in the eSMO lib source files).

Is there an EABI version of this eSMO library? If not, would it be possible to share the source files for this library? I could just recompile and build them as part of my F28004x project.
Thank you,
Hrishi