This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: Replacement for TMS320F28069MPZT

Part Number: TMS320F28069M

Hello, 

With given outages in shipping and short supply in parts, I am looking to replace the TMS320F28069MPZT on our boards with a suitable microcontroller. I would like to know which MCU which would best replace it without many changes to the PCB layout and the program code. Any assistance is appreciated. I see the part number: TMS320F28069FPFPQ which is available on Mouser, but it is an 80 Pin unit. Would it be direct swap for it in terms of code change? I need an MCU with at least 12 ADC input channels as we are looking to use the microcontroller for ADC sampling and processing. I am not using Instaspin on any of my application, so I would not be limited, but I am not sure if any other MCU would fit into our design. 

If I can get any help on this, that would be greatly appreciated.