Part Number: TMS320F280049
Hi Team,
May I know the detail GPIO status which will be changed in different boot mode if it is status not same as the reset status which describe in the TRM.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
Hi Team,
May I know the detail GPIO status which will be changed in different boot mode if it is status not same as the reset status which describe in the TRM.

Nima,
I don't use DCSM function.
You can consider my question is just for device which flash context is blank.
I guess I'm a bit confused. What are you trying to do with the GPIOs? Based on the status of them at RESET you perform different types of boot.
I just want to know for the blank chip, in each boot mode , which IO pin will be configured by TI Boot Rom code and the these IO pin detail status.
Customer need to know each mode IO status to decide the HW design. and choose the boot mode they needed.
I feel confused, this question is very hard to answer or not?
Okay on a blank chip It should be GPIO24 and GPIO32 and when the device powers up, these pins are in input mode and the device checks the status of them to see what boot mode you want. Thats why on our EVM, we put switches on these GPIOs so you can pick before you turn it on. Most users have it on 0b11 which is FLASH boot.
Sorry, i understand the boot mode pin and status.
What i want to know is the GPIO status which will be configured by Boot Rom code under different boot mode ?
For example, for CAN boot mode, except CAN pin any other GPIO will be configured by Boot Rom code?
Vivek Singh can you answer this about the boot rom?
For example, for CAN boot mode, except CAN pin any other GPIO will be configured by Boot Rom code?
Vivek Singh can you help answer below?
For example, for CAN boot mode, except CAN pin any other GPIO will be configured by Boot Rom code?
For example, for CAN boot mode, except CAN pin any other GPIO will be configured by Boot Rom code?
No, BOOTROM will only configure the pins which are used for specific peripheral.
Regards,
Vivek Singh