//###########################################################################
//
// FILE: 2802xI2C_non_FIFO_main.c
//
// TITLE: 2802x_I2C_non_FIFO_example
//
// ASSUMPTIONS:
//
// Add description here... TODO
//
// $Boot_Table
// While an emulator is connected to your device, the TRSTn pin = 1,
// which sets the device into EMU_BOOT boot mode. In this mode, the
// peripheral boot modes are as follows:
//
// Boot Mode: EMU_KEY EMU_BMODE
// (0xD00) (0xD01)
// ---------------------------------------
// Wait !=0x55AA X
// I/O 0x55AA 0x0000
// SCI 0x55AA 0x0001
// Wait 0x55AA 0x0002
// Get_Mode 0x55AA 0x0003
// SPI 0x55AA 0x0004
// I2C 0x55AA 0x0005
// OTP 0x55AA 0x0006
// Wait 0x55AA 0x0007
// Wait 0x55AA 0x0008
// SARAM 0x55AA 0x000A <-- "Boot to SARAM"
// Flash 0x55AA 0x000B
// Wait 0x55AA Other
//
// Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger
// according to the Boot Mode Table above. Build/Load project,
// Reset the device, and Run example
//
// $End_Boot_Table
//
// DESCRIPTION:
//
// This program will write 1-14 words to EEPROM and read them back.
// The data written and the EEPROM address written to are contained
// in the message structure, I2cMsgOut1. The data read back will be
// contained in the message structure I2cMsgIn1.
//
// This program will work with the on-board I2C EEPROM supplied on
// the F2802x eZdsp.
//
//
//###########################################################################
// $TI Release: F2802x Support Library v3.02.00.00 $
// $Release Date: Tue Jun 26 03:12:17 CDT 2018 $
// $Copyright:
// Copyright (C) 2009-2018 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
//
// I2C Function Prototypes
//
void I2CA_Init(void);
uint16_t I2CA_WriteToReg(uint16_t slave_addr, uint16_t reg,
uint16_t data[], uint16_t data_size);
uint16_t I2CA_WriteToManyRegs(uint16_t slave_addr, uint16_t reg[],
uint16_t reg_size, uint16_t data[], uint16_t data_size);
uint16_t I2CA_ReadFromReg(uint16_t slave_addr, uint16_t reg,
uint16_t data[], uint16_t data_size);
uint16_t I2CA_ReadFromManyRegs(uint16_t slave_addr, uint16_t reg[],
uint16_t reg_size, uint16_t data[], uint16_t data_size);
void InitI2CAGpio();
//
// Defines
//
#define I2C_SLAVE_ADDR 0x50
#define NACK_CHECK 1
//
// Globals
//
//
// Main
//
void main(void)
{
uint16_t Status, i;
//
// WARNING: Always ensure you call memcpy before running any functions from
// RAM InitSysCtrl includes a call to a RAM based function and without a
// call to memcpy first, the processor will go "into the weeds"
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
//
// Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f2802x_SysCtrl.c file.
//
InitSysCtrl();
//
// Setup only the GP I/O only for I2C functionality
//
InitI2CAGpio();
//
// Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the f2802x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in f2802x_DefaultIsr.c.
// This function is found in f2802x_PieVect.c.
//
InitPieVectTable();
//
// Initialize all the Device Peripherals
//
I2CA_Init(); // I2C-A only
//
// Define variables/buffers used for I2C comms
//
uint16_t reg[2]; // Register bytes buffer
uint16_t tx_data_buff[64]; // Data bytes buffer
uint16_t rx_data_buff[64]; // Data bytes buffer
// Define register bytes
reg[0] = 0x00;
reg[1] = 0x00;
// Define data bytes
for(i = 0; i <= sizeof(tx_data_buff); i++)
{
tx_data_buff[i] = i;
rx_data_buff[i] = 0;
}
// Transfer register and data bytes
Status = I2CA_WriteToManyRegs(I2C_SLAVE_ADDR, reg, sizeof(reg),
tx_data_buff, sizeof(tx_data_buff));
if(Status == I2C_SUCCESS)
{
Status = I2CA_ReadFromManyRegs(I2C_SLAVE_ADDR, reg, sizeof(reg),
rx_data_buff, sizeof(rx_data_buff));
while(Status != I2C_SUCCESS)
{
Status = I2CA_ReadFromManyRegs(I2C_SLAVE_ADDR, reg, sizeof(reg),
rx_data_buff, sizeof(rx_data_buff));
}
}
__asm(" ESTOP0");
}
//
// I2CA_Init -
//
void
I2CA_Init(void)
{
//
// I2CCLK = SYSCLK/(I2CPSC+1)
//
#if (CPU_FRQ_40MHZ||CPU_FRQ_50MHZ)
I2caRegs.I2CPSC.all = 4; // Prescaler - need 7-12 Mhz on module clk
#endif
#if (CPU_FRQ_60MHZ)
I2caRegs.I2CPSC.all = 6; // Prescaler - need 7-12 Mhz on module clk
#endif
// Set I2CCLKL/I2CCLKH for 100KHz SCL clock
I2caRegs.I2CCLKL = 38; // NOTE: must be non zero
I2caRegs.I2CCLKH = 38; // NOTE: must be non zero
I2caRegs.I2CIER.all = 0x0; // Disable interrupts
//
// Take I2C out of reset. Stop I2C when suspended
//
I2caRegs.I2CMDR.all = 0x0020;
return;
}
//
// InitI2CGpio - This function initializes GPIO pins to function as I2C pins
//
// Each GPIO pin can be configured as a GPIO pin or up to 3 different
// peripheral functional pins. By default all pins come up as GPIO
// inputs after reset.
//
// Caution:
// Only one GPIO pin should be enabled for SDAA operation.
// Only one GPIO pin shoudl be enabled for SCLA operation.
// Comment out other unwanted lines.
//
void
InitI2CAGpio()
{
EALLOW;
//
// Enable internal pull-up for the selected pins
// Pull-ups can be enabled or disabled disabled by the user.
// This will enable the pullups for the specified pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0; // Enable pull-up for GPIO32 (SDAA)
GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0; // Enable pull-up for GPIO33 (SCLA)
//
// Set qualification for selected pins to asynch only
// This will select asynch (no qualification) for the selected pins.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPBQSEL1.bit.GPIO32 = 3; // Asynch input GPIO32 (SDAA)
GpioCtrlRegs.GPBQSEL1.bit.GPIO33 = 3; // Asynch input GPIO33 (SCLA)
//
// Configure I2C pins using GPIO regs
// This specifies which of the possible GPIO pins will be I2C
// functional pins. Comment out other unwanted lines.
//
GpioCtrlRegs.GPBMUX1.bit.GPIO32 = 1; // Configure GPIO32 for SDAA
GpioCtrlRegs.GPBMUX1.bit.GPIO33 = 1; // Configure GPIO33 for SCLA
EDIS;
}
//
// I2CA_WriteToReg - This function writes data bytes to a slave
// device's register.
//
// INPUTS:
// - slave_addr ==> Address of slave device being written to
// - reg[] ==> Slave device register being written to
// - data[] ==> data buffer of bytes to be written to the slave
// device register
// - data_size ==> # of data bytes being written, size of data buffer
//
uint16_t I2CA_WriteToReg(uint16_t slave_addr, uint16_t reg,
uint16_t data[], uint16_t data_size)
{
uint16_t i, Status;
Status = I2C_SUCCESS;
//
// Wait until the STP bit is cleared from any previous master communication
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if (I2caRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
//
// Setup slave address
//
I2caRegs.I2CSAR = slave_addr;
//
// Check if bus busy
//
if (I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
//
// Set up as master transmitter
// FREE + MST + TRX + IRS
//
I2caRegs.I2CMDR.all = 0x4620;
//
// Setup number of bytes to send
// == register byte + (# of data[] buffer bytes)
//
I2caRegs.I2CCNT = 1 + data_size;
I2caRegs.I2CMDR.bit.STT = 0x1; // Send START condition
I2caRegs.I2CMDR.bit.STP = 0x1; // STOP condition will be
// generated when I2CCNT is zero
//
// I2C module will send the following:
// register byte ==> data bytes ==> STOP condition
//
while(!I2caRegs.I2CSTR.bit.XRDY){} // Make sure data
// is ready to be written
I2caRegs.I2CDXR = reg;
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
// Transmit Data Bytes followed by STOP condition
for (i=0; i< data_size; i++)
{
while(!I2caRegs.I2CSTR.bit.XRDY){} // Make sure data
// is ready to be written
I2caRegs.I2CDXR = data[i];
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
break;
}
#endif
}
// Data successfully written
return Status;
}
//
// I2CA_WriteToReg - This function writes data bytes to a slave
// device's register.
//
// INPUTS:
// - slave_addr ==> Address of slave device being written to
// - reg[] ==> Slave device registers being written to
// - reg_size ==> # of register bytes being written, size of
// reg_size buffer
// - data[] ==> data buffer of bytes to be written to the slave
// device register
// - data_size ==> # of data bytes being written, size of data buffer
//
uint16_t I2CA_WriteToManyRegs(uint16_t slave_addr, uint16_t reg[],
uint16_t reg_size, uint16_t data[], uint16_t data_size)
{
uint16_t i, Status;
Status = I2C_SUCCESS;
//
// Wait until the STP bit is cleared from any previous master communication
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if (I2caRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
//
// Setup slave address
//
I2caRegs.I2CSAR = slave_addr;
//
// Check if bus busy
//
if (I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
//
// Set up as master transmitter
// FREE + MST + TRX + IRS
//
I2caRegs.I2CMDR.all = 0x4620;
//
// Setup number of bytes to send
// == (# of register bytes) + (# of data[] buffer bytes)
//
I2caRegs.I2CCNT = reg_size + data_size;
I2caRegs.I2CMDR.bit.STT = 0x1; // Send START condition
I2caRegs.I2CMDR.bit.STP = 0x1; // STOP condition will be
// generated when I2CCNT is zero
//
// I2C module will send the following:
// register bytes ==> data bytes ==> STOP condition
//
// Transmit Register Bytes
for (i=0; i< reg_size; i++)
{
while(!I2caRegs.I2CSTR.bit.XRDY){} // Make sure data
// is ready to be written
I2caRegs.I2CDXR = reg[i];
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
}
// Transmit Data Bytes followed by STOP condition
for (i=0; i< data_size; i++)
{
while(!I2caRegs.I2CSTR.bit.XRDY){} // Make sure data
// is ready to be written
I2caRegs.I2CDXR = data[i];
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
}
// Data successfully written
return Status;
}
//
// I2CA_ReadFromReg - This function reads data bytes from a slave
// device's register.
//
// INPUTS:
// - slave_addr ==> Address of slave device being read from
// - reg ==> Slave device register being read from
// - data[] ==> data buffer to store the bytes read from the
// slave device register
// - data_size ==> # of data bytes being received, size of data buffer
//
uint16_t I2CA_ReadFromReg(uint16_t slave_addr, uint16_t reg,
uint16_t data[], uint16_t data_size)
{
uint16_t i, Status;
Status = I2C_SUCCESS;
//
// Wait until the STP bit is cleared from any previous master communication
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if (I2caRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
//
// Setup slave address
//
I2caRegs.I2CSAR = slave_addr;
//
// Check if bus busy
//
if (I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
//
// 1. Transmit the slave address followed by the register
// bytes being read from
//
//
// Setup number of bytes to send
// == # of register bytes
//
I2caRegs.I2CCNT = 1;
//
// Set up as master transmitter
// FREE + MST + TRX + IRS
//
I2caRegs.I2CMDR.all = 0x4620;
I2caRegs.I2CMDR.bit.STT = 0x1; // Send START condition
while(!I2caRegs.I2CSTR.bit.ARDY) // Wait for slave address to be sent
{
if(I2caRegs.I2CSTR.bit.XSMT == 0)
{
break;
}
}
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
// Transmit Register Byte
while(!I2caRegs.I2CSTR.bit.XRDY){} // Make sure data
// is ready to be written
I2caRegs.I2CDXR = reg;
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
// Wait for previous communication to complete
while(!I2caRegs.I2CSTR.bit.ARDY){}
//
// 2. Receive data bytes from slave device
//
//
// Set up as master receiver
// FREE + MST + IRS ==> (Master Receiver)
//
I2caRegs.I2CMDR.all = 0x4420;
//
// Setup number of bytes to receive
// == # of data bytes
//
I2caRegs.I2CCNT = data_size;
I2caRegs.I2CMDR.bit.STT = 0x1; // Send repeated START condition & Slave Addr
I2caRegs.I2CMDR.bit.STP = 0x1; // set STOP condition to be
// generated when I2CCNT is zero
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
for (i=0; i< data_size; i++)
{
while(!I2caRegs.I2CSTR.bit.RRDY){} // Make sure data
// is ready to be received
data[i] = I2caRegs.I2CDRR; // Buffer the received byte
}
// Data successfully read
return Status;
}
//
// I2CA_ReadFromManyRegs - This function reads data bytes from a slave
// device's registers. For transmitting more than one
// register during the initial writes
//
// INPUTS:
// - slave_addr ==> Address of slave device being read from
// - reg[] ==> Slave device registers being read from
// - reg_size ==> # of register bytes being written, size of
// reg_size buffer
// - data[] ==> data buffer to store the bytes read from the
// slave device register
// - data_size ==> # of data bytes being received, size of data buffer
//
uint16_t I2CA_ReadFromManyRegs(uint16_t slave_addr, uint16_t reg[],
uint16_t reg_size, uint16_t data[], uint16_t data_size)
{
uint16_t i, Status;
Status = I2C_SUCCESS;
//
// Wait until the STP bit is cleared from any previous master communication
// Clearing of this bit by the module is delayed until after the SCD bit is
// set. If this bit is not checked prior to initiating a new message, the
// I2C could get confused.
//
if (I2caRegs.I2CMDR.bit.STP == 1)
{
return I2C_STP_NOT_READY_ERROR;
}
//
// Setup slave address
//
I2caRegs.I2CSAR = slave_addr;
//
// Check if bus busy
//
if (I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
//
// 1. Transmit the slave address followed by the register
// bytes being read from
//
//
// Setup number of bytes to send
// == # of register bytes
//
I2caRegs.I2CCNT = reg_size;
//
// Set up as master transmitter
// FREE + MST + TRX + IRS
//
I2caRegs.I2CMDR.all = 0x4620;
I2caRegs.I2CMDR.bit.STT = 0x1; // Send START condition
while(!I2caRegs.I2CSTR.bit.ARDY) // Wait for slave address to be sent
{
if(I2caRegs.I2CSTR.bit.XSMT == 0)
{
break; // ACK received on slave address
}
}
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
// Transmit Register Bytes
for (i=0; i< reg_size; i++)
{
while(!I2caRegs.I2CSTR.bit.XRDY){} // Make sure data
// is ready to be written
I2caRegs.I2CDXR = reg[i];
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
}
// Wait for previous communication to complete
while(!I2caRegs.I2CSTR.bit.ARDY){}
//
// 2. Receive data bytes from slave device
//
//
// Set up as master receiver
// FREE + MST + IRS ==> (Master Receiver)
//
I2caRegs.I2CMDR.all = 0x4420;
//
// Setup number of bytes to receive
// == # of data bytes
//
I2caRegs.I2CCNT = data_size;
I2caRegs.I2CMDR.bit.STT = 0x1; // Send repeated START condition & Slave Addr
I2caRegs.I2CMDR.bit.STP = 0x1; // set STOP condition to be
// generated when I2CCNT is zero
#if NACK_CHECK // check if NACK was received
if(I2caRegs.I2CSTR.bit.NACK == 1)
{
I2caRegs.I2CMDR.bit.STP = 1;
I2caRegs.I2CSTR.all = I2C_CLR_NACK_BIT;
Status = I2C_ERROR;
return Status;
}
#endif
for (i=0; i< data_size; i++)
{
while(!I2caRegs.I2CSTR.bit.RRDY){} // Make sure data
// is ready to be received
data[i] = I2caRegs.I2CDRR; // Buffer the received byte
}
// Data successfully read
return Status;
}
//
// End of File
//
Hi
I don't understand the right way to manage NACK events. I have used an old sample of code (attached) in order to read a value from an i2c peripheral that at the moment is not connected. Of course I have NACK and the sw recognize the event but when it try to send a stop condition the BB bit become 1 and the MST goto 0. Next calls to I2CA_ReadFromReg the return always Bus BUsy error no other actions can be done on the bus.
Best Regards