Part Number: TMS320F280023
Other Parts Discussed in Thread: C2000WARE, , CODECOMPOSER, SYSCONFIG
Hi
The version number for C2000WARE version 4.00.00.00 is wrong after installing C2000WARE by used of the file C2000Ware_4_00_00_00_setup.exe downloaded from TI homepage.
In the file .metadata/sdk.json the version is set to "3.01.00.00", but I assume that it should be "4.00.00.00"
If you use the SysConig tool for setting up the device (e.g. TMS320F280023) it will shown the version 3.01.00.00 even through version 4.00.00.00 of C2000WARE was used.
First lines from file *.syscfg
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --device "F28002x" --package "48QFP" --part "F28002x_48QFP" --product "C2000WARE@3.01.00.00"
* @versions {"tool":"1.11.0+2225"}
*/
Best regards
Klaus Jensen