Part Number: TMS320F28027
Other Parts Discussed in Thread: TIDM-02011
Hi Champ,
I am asking for my customer. They are still using F28027 and looking forward to doing LFU through I2C.
The method of LFU with reset/without reset has been implemented on F28004x(TIDM-02011) and the later F28003x which devices has the two Flash banks.
Is it possible to do dual-image on a single-bank flash F28027/035 LFU through I2C?
I think to have dual images, one is programmed in factory (factory default image) and kept unchanged, the other is the updated (updated image) and the ISRs would need to run from RAM sounds feasible.
May I have any comment on this ?
Thanks and regards.