Part Number: TMS320F280023
Other Parts Discussed in Thread: SYSCONFIG
Q1: detailed datasheet TMS320F28002x: "spruin7a" page 799, TABLE 9-1 says that INPUT1 to INPUT14 (14 signals, looks like these signals are created once INPUT X-BAR is defined to respective GPIO signals) go to CLB X-BAR. Then in TABLE 9-4, page 803, I can see only INPUTXBAR1 to INPUTXBAR6 totalling 6 signals from INPUT X-BAR that can be used as input to CLB X-BAR. So, there is contradiction on 14 vs 6 signals. Please clarify.