Hi,
I was using two buck converters in parallel and the Top Buck Converter is working well.
Now, I copied the control code of the Top Buck converter and used for bottom-buck converter with different names.
Build Done Successfully but after debugging it shows the following error.
Please help me
(Error -1142 @ 0x0)
Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation.
(Emulation package 8.4.0.00006)
Thank You