Part Number: TMDSCNCD28379D
Is it possible to have both debug and Serial communication over J1 USB connecter simultaneously?
Page 9 of the user guide states the following, suggesting that this is possible. If not, then I will need to add a separate serial connector to an interface board using other dedicated serial pins on the HSEC180 connector.
"Emulation/UART connector - USB mini A connector used to provide xds100v2 emulation and USB-to-UART(SCI) communication through FTDI logic. A:SW1 determines which connections are enabled to the MCU."
Thank you
Erik