This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSDOCK28069: Operating ambient temperature of development kit

Part Number: TMDSDOCK28069


Hi Experts,

Good day.

Device: TMDSDOCK28069

I couldn't find related document to confirm its operating ambient temperature of this dev't board.

Can you please confirm?

Thank you.

Regards,
Archie A.

  • Archie,

          The ControlCard is only an evaluation platform and is not meant to be used in an end-product. It is typically used for code-development. Do you know customer's motivation for asking this information? Typically, temperature rating is evaluated only for production designs. 

  • Archie,

    this is intended to operate at STP, or ~20C. We do not require all devices on the evaluation kit to run across the same temperature range as the F2806x device.

    As Hareesh mentioned we do not recommend this for use in an end product, I recognize some customers do however like to do temperature characterization. The PCB material is FR4, so it should support a wide temperature range, but other devices on the board may deteriorate. 

    Regards,
    Cody